How do I change the display to use RGB24 instead of RGB666 in U-boot 2009.08?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I change the display to use RGB24 instead of RGB666 in U-boot 2009.08?

1,550 次查看
micschrag
Contributor IV

Please refer to this post:

How do I change the display to use RGB24 instead of RGB666 in U-boot 2009.08?

It has not been answered although marked "Assumed Answered". Please keep offering suggestions on the above post.

标签 (2)
0 项奖励
回复
2 回复数

1,329 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

1,329 次查看
micschrag
Contributor IV

Igor,

The patch says that it is for the JB4.2.2-1 BSP, and we are using KK4.4.2 BSP. Is this a problem for the patcher, or were there no major changes between the two releases? Furthermore, when we built our work environment, we did apply a patch (as instructed by Freescale).  I am not sure if this patch accomplished the same changes that you recommend. From the "How-To" manual:

"

     .../uboot-imx$ cd /android/WorkArea/

     .../WorkArea/$ source /android/android_kk4.4.2_1.0.0-ga_core_source/code/kk4.4.2_1.0.0-ga/and_patch.sh

     .../WorkArea/$ help //"c_patch" function should be visible

     .../WorkArea/$ c_patch /android/android_kk4.4.2_1.0.0-ga_core_source/code/kk4.4.2_1.0.0-ga imx_kk4.4.2_1.0.0-ga

     Should see SUCCESS: Now you can build the Android code for FSL i.MX platform

"

-Michael

Edit: This seems to indicate to me that we have already applied the patch. Is there another solution we can try?

0 项奖励
回复