How configure and use acm and adb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How configure and use acm and adb

7,469 Views
marekbil
Contributor I

Hi, i can't use acm. If i use acm if i switch adb on/off system not run.

Mu init.usb.rc

# Copyright 2013 The Android Open Source Project
#
# Licensed under the Apache License, Version 2.0 (the "License");
# you may not use this file except in compliance with the License.
# You may obtain a copy of the License at
#
#      http://www.apache.org/licenses/LICENSE-2.0
#
# Unless required by applicable law or agreed to in writing, software
# distributed under the License is distributed on an "AS IS" BASIS,
# WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
# See the License for the specific language governing permissions and
# limitations under the License.

on init
    write /sys/class/android_usb/android0/f_rndis/manufacturer Freescale
    write /sys/class/android_usb/android0/f_rndis/vendorID 18D1
    write /sys/class/android_usb/android0/f_rndis/wceis 1

    mount configfs none /config
    mkdir /config/usb_gadget/g1
    write /config/usb_gadget/g1/idVendor 0x18d1
    write /config/usb_gadget/g1/idProduct 0x4e42
    mkdir /config/usb_gadget/g1/strings/0x409
    write /config/usb_gadget/g1/strings/0x409/serialnumber 0123459876
    write /config/usb_gadget/g1/strings/0x409/manufacturer test
    write /config/usb_gadget/g1/strings/0x409/product nv1

    mkdir /config/usb_gadget/g1/configs/c.1
    mkdir /config/usb_gadget/g1/configs/c.1/strings/0x409
    write /config/usb_gadget/g1/configs/c.1/strings/0x409/configuration "cdc 2xACM+ECM"


    mkdir /config/usb_gadget/g1/functions/acm.GS0
    mkdir /config/usb_gadget/g1/functions/acm.GS1
    mkdir /config/usb_gadget/g1/functions/acm.usb0


#    ln -s /config/usb_gadget/g1/functions/acm.GS0  /config/usb_gadget/g1/configs/c.1
#    ln -s /config/usb_gadget/g1/functions/acm.GS1  /config/usb_gadget/g1/configs/c.1
#    ln -s /config/usb_gadget/g1/functions/ecm.usb0  /config/usb_gadget/g1/configs/c.1


on boot
    write /sys/class/android_usb/android0/iSerial $ro.serialno
    write /sys/class/android_usb/android0/iManufacturer $ro.product.manufacturer
    write /sys/class/android_usb/android0/iProduct $ro.product.model

on fs
    mkdir /dev/usb-ffs 0770 shell shell
    mkdir /dev/usb-ffs/adb 0770 shell shell
    mount functionfs adb /dev/usb-ffs/adb uid=2000,gid=2000
    write /sys/class/android_usb/android0/f_ffs/aliases adb

# USB rndis configuration
on property:sys.usb.config=rndis
    stop adbd
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 4e23
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/bDeviceClass 224
    write /sys/class/android_usb/android0/enable 1
    setprop sys.usb.state ${sys.usb.config}

on property:sys.usb.config=mtp
    stop adbd
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 4e41
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/f_acm/instances 2
    write /sys/class/android_usb/android0/enable 1
    setprop sys.usb.state ${sys.usb.config}

on property:sys.usb.config=mtp,acm
    stop adbd
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 2513
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/f_acm/instances 2
    write /sys/class/android_usb/android0/enable 1
    setprop sys.usb.state ${sys.usb.config}


on property:sys.usb.config=mtp,adb

    stop adb
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 4e42
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/enable 1
    start adbd
    write /config/usb_gadget/g1/UDC ci_hdrc.0
    
    setprop sys.usb.state ${sys.usb.config}

on property:sys.usb.config=mtp,acm,adb
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 2514
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/f_acm/instances 2
    write /sys/class/android_usb/android0/enable 1
    start adbd
    setprop sys.usb.state ${sys.usb.config}


on property:sys.usb.config=ptp
    stop adbd
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 4e43
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/enable 1
    setprop sys.usb.state ${sys.usb.config}

on property:sys.usb.config=ptp,adb
    write /sys/class/android_usb/android0/enable 0
    write /sys/class/android_usb/android0/idVendor 18d1
    write /sys/class/android_usb/android0/idProduct 4e44
    write /sys/class/android_usb/android0/functions ${sys.usb.config}
    write /sys/class/android_usb/android0/enable 1
    start adbd
    setprop sys.usb.state ${sys.usb.config}

How can i use acm and adb ?

0 Kudos
Reply
1 Reply

3,726 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hi,    add the following lines in init.freescale.usb.rc

 

on property:sys.usb.config=mtp,adb,acm

    write /sys/class/android_usb/android0/enable 0

    write /sys/class/android_usb/android0/idVendor 18d1

    write /sys/class/android_usb/android0/idProduct d02

    write /sys/class/android_usb/android0/functions $sys.usb.config

    write /sys/class/android_usb/android0/f_acm/instances 1

    write /sys/class/android_usb/android0/enable 1

    start adbd

    setprop sys.usb.state $sys.usb.config

 

along with this it needs one more line in

default.prop  i.e   change persist.sys.usb.config=mtp,adb   to  persist.sys.usb.config=mtp,adb,acm  it will work.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply