How can use Imx6ull pwm pin in kernel and userspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can use Imx6ull pwm pin in kernel and userspace

2,710件の閲覧回数
analogicstechin
Contributor III

HI ,

 I am using imx6ull  pwm pin using in kernel space but unable to use in user space is there any possibility guide me.

below PIN is my custom board connected to buzzer.

MX6UL_PAD_GPIO1_IO09__PWM2_OUT 

please guide us to use buzzer play in user space.

ラベル(1)
0 件の賞賛
返信
1 返信

2,235件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

for linux pwm driver description one can look at Chapter 47 Pulse-Width Modulator

(PWM) Driver, overview on

imx6s PWM sysfs 

PWM (Linux) 

linux/arch/arm/boot/dts/imx6ull-14x14-evk.dts

imx6ull-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信