How can i trigger a software reset from u-boot WITHOUT using watchdog timer?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i trigger a software reset from u-boot WITHOUT using watchdog timer?

ソリューションへジャンプ
3,946件の閲覧回数
aasheesh
Contributor I

Please let me know how to trigger a software reset from u-boot without using watchdog timer.

ラベル(2)
0 件の賞賛
返信
1 解決策
3,674件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aasheesh

one can use WCR_SRS bit : writing to &wdog->wcr  in

u-boot/imx_watchdog.c at master · mripard/u-boot · GitHub

WDOGx_WCR, SRS - Software Reset Signal,

sect.70.7.1 Watchdog Control Register (WDOGx_WCR) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aasheesh

one can use WCR_SRS bit : writing to &wdog->wcr  in

u-boot/imx_watchdog.c at master · mripard/u-boot · GitHub

WDOGx_WCR, SRS - Software Reset Signal,

sect.70.7.1 Watchdog Control Register (WDOGx_WCR) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,674件の閲覧回数
aasheesh
Contributor I

Thank you for your prompt reply.But in my board the watchdog is not connected to the PMIC. So,even if i set the WCR_SRS bit,i think it will not do a reset.Is there any alternative method which does not use watchdog like maybe SRC register or something like that.

0 件の賞賛
返信
3,674件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

WCR_SRS will reset processor without usage of PMIC.

0 件の賞賛
返信
3,674件の閲覧回数
aasheesh
Contributor I

Thank you.By deasserting the SRS bit,my reset works.However,I must first disable warm_reset_enable bit in SRC_SCR register.The problem in my board was that WDOG_B was not connected to PMIC,so a watchdog timeout will not reset the PMIC. I have made an observation.Please let me know whether i am correct.I think deasserting the SRS bit creates a warm reset but as my warm_reset_enable bit is disabled,all warm reset sources must generate a cold reset.Hence my warm reset is actually creating a cold reset.Is it correct?Thank you for your assistance. Looking forward for your reply.

0 件の賞賛
返信
3,674件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I think your understanding is right.

0 件の賞賛
返信