How can i.mx8 booting from qspi?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i.mx8 booting from qspi?

Jump to solution
2,382 Views
linux_downey
Contributor III

Hi :

      I'm developing on i.mx8mq evk board,and I find it has a QuadSPI. I'm trying to boot from QuadSPI with my i.mx8mq

      evk board, I have took operations below:

      1. Compile a bootloader which named flash.bin, This flash.bin is available( running OK on emmc).

      2. Use uuu tool to burn the flash.bin to qspi with instructions below:

                  uuu -b qspi flash.bin

          from the debug port ,it seems excutes OK!

      3. Looking for the DIP switch settings in  document (linux user guide—— section——4.5.10),I can't find the

            settings for i.mx8,only for i.mx6&7 board.  So ,when I repower ,there is no debug log output.

         

         And I also have no idea that how to download a kernel Image to qspi.

        

        Please give me some signals of how to boot from qspi,thanks a lot!

Best Regards.

Downey.

Tags (1)
0 Kudos
Reply
1 Solution
2,149 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I have confirmed for you that, no setting for boot from QSPI on the i.MX8MQ board in our user guide document. So here do not  recommend you to use the QSPI boot up. You can use the emmc or SD card.

Have a nice day

Rita

View solution in original post

3 Replies
2,149 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version BSP are you using?

0 Kudos
Reply
2,149 Views
linux_downey
Contributor III

The version is 4.14.98

0 Kudos
Reply
2,150 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I have confirmed for you that, no setting for boot from QSPI on the i.MX8MQ board in our user guide document. So here do not  recommend you to use the QSPI boot up. You can use the emmc or SD card.

Have a nice day

Rita