How can i evaluate the image processing and video encoding performance of IPU and VPU of i.mx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i evaluate the image processing and video encoding performance of IPU and VPU of i.mx6

1,592件の閲覧回数
ntrikoti
Contributor I

Hi all,

We are planning to use i.mx6D processor for our camera application. we are capturing the image data using cmos sensor which gives 12bit bayer data. This bayer data shall be converted to YUVA and then to YUV420 to give it to VPU to encode it to h.264 format.

Here in the above scenario my consern is can we use IPU of i.mx6 for conversion from bayer to YUVA and YUVA to YUV420. IF yes please direct me to proper link.

What is the achievable frame rate with respect to above scenario and what shall be the approximate timings for the above mentioned conversions and video encoding for HD image (1080x1920).

Any kind of help is greatly appreciated.

Thanks.

ラベル(3)
0 件の賞賛
返信
1 返信

1,439件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the link as below:

<Re: IPU - bayer pattern conversion >

0 件の賞賛
返信