How can configure ESAI to I2S mode in i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can configure ESAI to I2S mode in i.MX6?

ソリューションへジャンプ
2,563件の閲覧回数
JHY
Contributor IV

There are 3 x I2S ports in IMX6 and I consider one more I2S, so decided to use ESAI.

Where can I find the way to configure ESAI to I2S mode?

Is there an reference schematic or example code ?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,614件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for ESAI I2S programming one can look at

sect.4.3.1 INTER-IC SOUND (I2S) FORMAT

http://cache.freescale.com/files/dsp/doc/app_note/AN1848.pdf

and reuse SDK ESAI audio example (imx_esai.c)

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,615件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for ESAI I2S programming one can look at

sect.4.3.1 INTER-IC SOUND (I2S) FORMAT

http://cache.freescale.com/files/dsp/doc/app_note/AN1848.pdf

and reuse SDK ESAI audio example (imx_esai.c)

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信