How can be estimated the power consumption in a processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can be estimated the power consumption in a processor

1,511 Views
abelardonavarro
Contributor I

The power dissipation in a complex system depends on the process the system is doing. In a processor this highly stocastic. In this case the easier way is to measure the current in the core's power supply. However sometime it is better have an estimation prior to having a coplete code to evaluate. Is it a way that can be estimated?

Labels (2)
0 Kudos
Reply
1 Reply

1,292 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abelardo

estimation for Cortex A9 : 0.25 mW/Mhz

(250mW @ 1GHz) per http://www.arm.com/products/processors/cortex-a/cortex-a9.php

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply