How can be estimated the power consumption in a processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can be estimated the power consumption in a processor

1,068 次查看
abelardonavarro
Contributor I

The power dissipation in a complex system depends on the process the system is doing. In a processor this highly stocastic. In this case the easier way is to measure the current in the core's power supply. However sometime it is better have an estimation prior to having a coplete code to evaluate. Is it a way that can be estimated?

标签 (2)
0 项奖励
回复
1 回复

849 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abelardo

estimation for Cortex A9 : 0.25 mW/Mhz

(250mW @ 1GHz) per http://www.arm.com/products/processors/cortex-a/cortex-a9.php

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复