How can be estimated the power consumption in a processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can be estimated the power consumption in a processor

1,052件の閲覧回数
abelardonavarro
Contributor I

The power dissipation in a complex system depends on the process the system is doing. In a processor this highly stocastic. In this case the easier way is to measure the current in the core's power supply. However sometime it is better have an estimation prior to having a coplete code to evaluate. Is it a way that can be estimated?

ラベル(2)
0 件の賞賛
返信
1 返信

833件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abelardo

estimation for Cortex A9 : 0.25 mW/Mhz

(250mW @ 1GHz) per http://www.arm.com/products/processors/cortex-a/cortex-a9.php

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信