How can I use preview and capture at the same time?(BT.656)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I use preview and capture at the same time?(BT.656)

1,695 次查看
donggyulee
Contributor I

Hi,

I have some questions.

How can I use preview and capture at the same time?

1. Video Input format is BT.656.

2. The Input Resolution is 1080P.

3. The Output(Preview) Resolution is 1080P(to HDMI)

4. Capture Resolution is 1080P(for H.264 Encoding).

AP  :  i.mx6q 1Ghz

RAM : DDR3 528Mhz

Storage : SSD 128GB

OS : Linux 3.0.101

is it Possible?

if possible, please advise.

Thanks.


Have a Nice Day!

0 项奖励
回复
4 回复数

1,546 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

please look at unit tests example and description in

..mxc_v4l2_test/doc/FSL-UT-V4L2-001.txt

Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,546 次查看
donggyulee
Contributor I

Hi igor

Thanks you so much

i will try

by the way

Is it possible for the 1080P Preview(30FPS) and Recording(30FPS) at the same time?

Thank you

0 项奖励
回复

1,546 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

I think yes.

Best regards

igor

0 项奖励
回复

1,546 次查看
donggyulee
Contributor I

Hi igor

okay i will try.

Thank you

Have a nice day

0 项奖励
回复