How can I test JB4.3 “webrtc(web real-time communication)” function in i.MX6Q Sabre SD?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I test JB4.3 “webrtc(web real-time communication)” function in i.MX6Q Sabre SD?

跳至解决方案
8,707 次查看
yangruihero
NXP Employee
NXP Employee

Dear:

I have found that JB4.3 has added new "webrtc" feature in "i.MX6 android_jb4.3_1.0.0 Android Release Notes", could you please provide some detailed information about this function?

How can I test JB4.3 "webrtc(Web real-time communication)" function in i.MX6Q Sabre-SD?

Thank you very much!

标签 (2)
1 解答
7,861 次查看
max_tsai
NXP Employee
NXP Employee

hi,

According to the log, that seems to be related with chromium browser. These is a similar open issue on chromium.

http://code.google.com/p/chromium/issues/detail?id=362348

Regards,

Max

在原帖中查看解决方案

0 项奖励
回复
16 回复数
7,861 次查看
norisugi
Contributor II

I tested the WebRTC using the Chrome with UVC USB Camera.

Then the browser crash occurred.

It seems that audio driver crash.

I attach the adb log.

Could you check it ?

0 项奖励
回复
7,862 次查看
max_tsai
NXP Employee
NXP Employee

hi,

According to the log, that seems to be related with chromium browser. These is a similar open issue on chromium.

http://code.google.com/p/chromium/issues/detail?id=362348

Regards,

Max

0 项奖励
回复
7,861 次查看
norisugi
Contributor II

Currently I can't judge whether this issue is due to the browser or not.

I got the another adb log.

Could you check the attached file ?

0 项奖励
回复
7,861 次查看
max_tsai
NXP Employee
NXP Employee

Your attached log also looks similar as Issue 362348 - chromium - [Android-WebRTC] Crash in accessing WebRTC page with external USB camera -...

--

I/DEBUG   ( 2358): backtrace:

I/DEBUG   ( 2358):     #00  pc 0001e684  /system/lib/libc.so

I/DEBUG   ( 2358):     #01  pc 0001c550  /system/lib/libc.so (abort+4)

I/DEBUG   ( 2358):     #02  pc 000121f1  /system/lib/libc.so

I/DEBUG   ( 2358):     #03  pc 00011701  /system/lib/libc.so (__assert2+20)

I/DEBUG   ( 2358):     #04  pc 01bf1649  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #05  pc 01bf173d  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #06  pc 01bf3c6b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #07  pc 01aad261  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #08  pc 01a9a74b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #09  pc 01ab2d9b  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #10  pc 01aab13d  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #11  pc 00b82601  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

I/DEBUG   ( 2358):     #12  pc 00b7fe33  /data/app-lib/org.chromium.chrome.shell-1/libchromeshell.so

--

Regards,

Max

0 项奖励
回复
7,861 次查看
norisugi
Contributor II

Thank you for your information.

My issue has been fixed by the workaround of the WebRTC project.

Many thanks !

0 项奖励
回复
7,861 次查看
EricNelson
Senior Contributor II

Hi Nori,

Do you have a reference to the fix?

0 项奖励
回复
7,861 次查看
norisugi
Contributor II
7,861 次查看
EricNelson
Senior Contributor II

Thanks Nori.

0 项奖励
回复
7,861 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

MaxTsai can you continue with the  follow up?

0 项奖励
回复
7,861 次查看
YixingKong
Senior Contributor IV

Rui

Since there is no reply from you, I am closing the DI. If your issue still exists please come here again and reopen the DI.

Thanks,

Yixing

0 项奖励
回复
7,861 次查看
YixingKong
Senior Contributor IV

Rui, are you ok to close the DI?

Thanks,

Yixing

0 项奖励
回复
7,861 次查看
EricNelson
Senior Contributor II

Actually, this doesn't answer the question, it just brings up another:

How do you install Chrome?

(Chrome isn't a part of the stock build)

We've tested WebRTC successfully in the 4.2-beta using the Mozilla Fennec browser

as described here:

     http://boundarydevices.com/second-release-jellybean-4-3-beta-mx6/

0 项奖励
回复
7,861 次查看
max_tsai
NXP Employee
NXP Employee

Sure, you can use firefox browser for Android instead of Chrome. That blog shows how to use Firefox also.

Since Mozilla starts to support webRTC since Firefox 24, you can install lastest Firefox for Android without Aurora.

Then you test by Mozilla gUM test page as you describes in your http://boundarydevices.com/second-release-jellybean-4-3-beta-mx6/

Or you can test by palava.tv

7,861 次查看
EricNelson
Senior Contributor II

:smileyhappy: And the https://palava.tv/test URL is much easier to type!

0 项奖励
回复
7,861 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

MaxTsai please continue with the follow up.

0 项奖励
回复