Hello,
i want to work with a screen that is not in MXC_lcdif.c file.
So I made the following changes in mxc_lcdif.
{
/* 480x272 @ 60 Hz , pixel clk @ 9MHz */
"CLAA-WVGA", 60, 480, 272, 100000, 8, 2, 11, 2, 35, 2,
//nane , refresh, xres, yres,pixclock, leftmargin, rightmargin, uppermargin, lowermargin, hsync, vsync
FB_SYNC_CLK_LAT_FALL, //sync
FB_VMODE_NONINTERLACED, //vmode
0,},
/* 800x480 @ 57 Hz , pixel clk @ 27MHz */
/*"CLAA-WVGA", 57, 800, 480, 37037, 40, 60, 10, 10, 20, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},*/
{
/* 800x480 @ 60 Hz , pixel clk @ 32MHz */
/*"SEIKO-WVGA", 60, 800, 480, 29850, 89, 164, 23, 10, 10, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},*/
But, I can not build the kernel. How can i compile kernel?