How can I program MMPF0100NP to F0 mode in u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I program MMPF0100NP to F0 mode in u-boot?

Jump to solution
1,569 Views
JHY
Contributor IV

In u-boot console, I excuted 'i2c probe' and confirmed communication with PMIC(0x08 i2c line).

But there are so many parameters that I have a hard time to test.

If there are references for setting PMIC to F0 mode, please tell me how can I get them.

Best regards.

0 Kudos
Reply
1 Solution
1,211 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

please refer to

AN4536 AN4536, MMPF0100 OTP Programming Instructions - Application Note

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,212 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

please refer to

AN4536 AN4536, MMPF0100 OTP Programming Instructions - Application Note

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply