How can I increase network speed in u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I increase network speed in u-boot?

Jump to solution
1,935 Views
JHY
Contributor IV

How can I increase network speed in u-boot?

Labels (1)
0 Kudos
Reply
1 Solution
1,565 Views
igorpadykov
NXP Employee
NXP Employee

HI JHY

also it is necessary to verify that server uses gigabit switch,

one can check negotiated speed using link:

[U-Boot] AR8031 Ethernet on mx6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,566 Views
igorpadykov
NXP Employee
NXP Employee

HI JHY

also it is necessary to verify that server uses gigabit switch,

one can check negotiated speed using link:

[U-Boot] AR8031 Ethernet on mx6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply