How can I get pre-written image of MIMXRT595EVK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I get pre-written image of MIMXRT595EVK?

ソリューションへジャンプ
721件の閲覧回数
tomi3
Contributor II

Hi,

I am using MIMXRT595EVK and G1120BOMIPI display.

While working and trying some examples, I'm getting confused whether EVK work well or not.

So, I want to return EVK to the original state, how can I get pre-written image (e.g. blinky) of MIMXRT595EVK?

Any help would be appreciated.

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
700件の閲覧回数
tomi3
Contributor II

Problem with not being able to write to EVK was solved.

Sorry for my misunderstanding isp mode config. (2-1-0 / 0-1-2)

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
713件の閲覧回数
tomi3
Contributor II

The current situation is like as follows.

---

Error in final launch sequence:

Failed to execute MI command:
-target-download
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
-target-download
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

0 件の賞賛
返信
701件の閲覧回数
tomi3
Contributor II

Problem with not being able to write to EVK was solved.

Sorry for my misunderstanding isp mode config. (2-1-0 / 0-1-2)

 

0 件の賞賛
返信