How can I execute code in ram directly by MFGTOOL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I execute code in ram directly by MFGTOOL?

ソリューションへジャンプ
2,209件の閲覧回数
weifeng2
Contributor I

hello,

I designed a new board based on imx6ul ,and the board has a UART and USB_OTG port. I have made a image to confirm whether the UART port commication is good,of course the image has already contained essential IVT info to intit the DRAM and clock ,etc.
Now,I want to load the image to DRAM by USB_OTG port and let it run imediatly,I used the MFGTOOL and modified the ucl2.xml document as follows:

 <LIST name="imx6ul-test" desc="RUN IN RAM">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/image.img" ifdev="MX6UL">Loading image</CMD>
<CMD state="BootStrap" type="jump" > Jumping to my image. </CMD>
</LIST>

The MFGTOOL log says "Jump to Ramkernel successfully!" , but my PC UART software has nothing happened,why does it not work? Is my image code problem or this download means is wrong?

ラベル(3)
0 件の賞賛
返信
1 解決策
2,055件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wei

application images in MFG2 Tool folder are images with offset -
written for programming on external boot devices. For USB
load one needs to use images, but without offset.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,056件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wei

application images in MFG2 Tool folder are images with offset -
written for programming on external boot devices. For USB
load one needs to use images, but without offset.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,055件の閲覧回数
weifeng2
Contributor I

Ok, Thanks for your answer. I will try it on my board.

0 件の賞賛
返信