How can I catch a SGI in Linux in an AMP system?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I catch a SGI in Linux in an AMP system?

4,958 次查看
christoph8446
Contributor II

Hello,

I have a dual core system. On Core 0 I use Linux and on Core 1 I use a Bare Metal System. I send a software generated interrupt from my Bare Metal System to Linux but I cannot catch the interrupt in Linux. How can I register a SGI interrupt in Linux? Request_irq() returns an error for SGI’s..

Thanks!

标签 (5)
8 回复数

4,406 次查看
wangzhimin
Contributor II

Did you solved this problem, I also encountered this problem

0 项奖励
回复

4,406 次查看
christoph8446
Contributor II

Yes, I got it. In the directory /arch/arm/kernel/smp.c you can find the function handle_IPI. There is a SWITCH CASE inside the function where you can add a new case for your IPI. The case number is equal to IPI number!

 

Regards

Chris

4,406 次查看
wangzhimin
Contributor II

If I need to use SGI to capture an interrupt in both cores in AMP mode, do I need to register the interrupt function in both cores separately, will this interfere?

Thanks.

0 项奖励
回复

4,406 次查看
christoph8446
Contributor II

I use the IPI only in one direction from bare-metal to linux. Maybe you can search for something like send IPI in linux sources...

In my opinion you must register the interrupt function in both cores separately.

0 项奖励
回复

4,406 次查看
mihaitaivascu
Contributor III

Hi Chris,

    How did you registered the irq handler on Linux side? You have an example?

    Is it correct to use SMP handle_IPI in AMP scheme?

    I have the same requirements as the ones described in this topic.

    request_irq does not work for me I get -22 error and I have the SGI defined in intc node in device tree.

    I need to catch it in some device driver.

Best regards,

         Mihaita

0 项奖励
回复

4,406 次查看
wangzhimin
Contributor II

Thank you for your answer, and I would like to ask another question. What API to use in a linux system to interrupt a bare-metal system.
Thanks again.

0 项奖励
回复

4,406 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chris

seems this is not supported in bsp, one can look at suggestions on

Inter processor Interrrupts in ARM cortex A9 ( How To write an handler for Software generated Interr... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,406 次查看
christoph8446
Contributor II

Hi Igor,

Thanks for your reply. I have looked at your link and I think the solution in the link was that they used the function set_ipi_handlers instead of request_irq. The function set_ipi_handlers is from XILINX BSP and not available in freescale's /smp.c. There should be a way to register an ISR for interrupt 0..15 (SGI).

Regards

Chris

0 项奖励
回复