I have an IMX6ULL EVM board, and this is my EVM kernel info
ID="fsl-imx-xwayland"
NAME="NXP i.MX Release Distro"
VERSION="4.9.88-2.0.0 (rocko)"
VERSION_ID="4.9.88-2.0.0"
PRETTY_NAME="NXP i.MX Release Distro 4.9.88-2.0.0 (rocko)"
when I connect an usb uvc camera on the EVM board, and the system find the camera info
new high-speed USB device number 5 using ci_hdrc
uvcvideo: Found UVC 1.00 device USB Camera (0bda:3035)
input: USB Camera as /devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1
/usb2/2-1/2-1.3/2-1.3:1.0/input/input6
I have use "v4l2-ctl --list-devices" to find my devices
USB Camera (usb-ci_hdrc.1-1.3):
/dev/video2
1. How can I turn on the camera? and get the video data?
2. How to Send out the camera data through internet (http or udp protocol) ?