How can ı load a new dtb file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can ı load a new dtb file

6,348 次查看
dugurlu
Contributor I

Hello everyone,

I want to change my dtb file on u-boot screen. Firstly ı loaded new dtb file with xmodem. 

loadx ${fdt_addr} ${fdt_file} 

fdt addr 0x18000000

This commands works. I can see the new dtb on u-boot console screen with fdt print. But ı couldn't save MMC dev 1 the new dtb file. How can ı do it? Here is my command for write MMC dev 1.

mmc dev ${mmcdev}; mmc rescan; setexpr blkc ${filesize} / 0x200; setexpr blkc ${blkc} + 1; if itest ${blkc} <= ${fdt_size}; then mmc write ${loadaddr} ${fdt_start} ${blkc};fi

Output is  "Error: card is write protected!" 

Here is my environment variables:

=> printenv
addcma=setenv bootargs ${bootargs} cma=${cma_size}
addfb=setenv bootargs ${bootargs} consoleblank=0 video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24
addip=if test "${ipmode}" != static; then run addip_dynamic; else run addip_static; fi
addip_dynamic=setenv bootargs ${bootargs} ip=dhcp
addip_static=setenv bootargs ${bootargs} ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}:${netdev}:off
addmmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p${mmcpart} ${rootfsmode} rootwait
addnfs=setenv bootargs ${bootargs} root=/dev/nfs rw nfsroot=${serverip}:${rootpath},v3,tcp;
addtty=setenv bootargs ${bootargs} console=${console},${baudrate} quiet vt.global_cursor_default=0
baudrate=115200
board=tqma6
board_name=TQMa6Q
boardtype=TQMa6Q-AA.0202
boot_dev=mmc
boot_type=bootz
bootcmd=run mmcboot; run netboot; run panicboot
bootdelay=3
cma_size=256M
console=ttymxc1
ethact=FEC
ethaddr=00:d0:93:37:dd:bf
ethprime=FEC
fbdepth=32
fbdrv=imxdrm
fdt_addr=0x18000000
fdt_file=imx6q-mba6x.dtb
fdt_high=0xffffffff
fdt_name=if test "${fdt_type}" != single; then setenv fdtimg ${fitfdt_file}; else setenv fdtimg ${fdt_file}; fi
fdt_size=0x800
fdt_start=0x1000
fdt_type=single
fitfdt_file=imx6q-mba6x.dtb.fit
fitfdt_part=fdt@0
get_fdt=run fdt_name; if test "${fdt_type}" != single; then echo use dtb from fit; if ${getcmd} ${loadaddr} ${fdtimg}; then imxtract ${loadaddr} ${fitfdt_part}${fdt_addr}; fi; else echo use dtb; ${getcmd} ${fdt_addr} ${fdtimg}; fi; setenv fdtimg
initrd_high=0xffffffff
ipmode=static
kernel_name=if test "${boot_type}" != bootz; then setenv kernel ${uimage}; else setenv kernel ${zimage}; fi
kernel_size=0x2000
kernel_start=0x2000
loadaddr=0x12000000
loadfdt=if test "${fdt_type}" != single; then run loadfdtfit; else run loadfdtsingle; fi
loadfdtfit=mmc dev ${mmcdev}; mmc read ${loadaddr} ${fdt_start} ${fdt_size}; imxtract ${loadaddr} ${fitfdt_part} ${fdt_addr}
loadfdtsingle=mmc dev ${mmcdev}; mmc read ${fdt_addr} ${fdt_start} ${fdt_size};
loadimage=mmc dev ${mmcdev}; mmc read ${loadaddr} ${kernel_start} ${kernel_size};
mmcargs=run addmmc addtty addfb addcma
mmcblkdev=1
mmcboot=echo Booting from mmc ...; setenv bootargs; run mmcargs; if run loadfdt; then echo boot device tree kernel ...; if run loadimage; then ${boot_type} ${loadaddr} - ${fdt_addr}; fi; else if run loadimage; then ${boot_type}; fi; fi;
mmcdev=1
mmcpart=3
netargs=run addnfs addip addtty addfb addcma
netboot=echo Booting from net ...; run kernel_name; run set_getcmd; setenv bootargs; run netargs; if run get_fdt; then if ${getcmd} ${loadaddr} ${kernel}; then ${boot_type} ${loadaddr} - ${fdt_addr}; fi; fi; echo ... failed
netdev=eth0
panicboot=echo No boot device !!! reset
rootfsmode=ro
rootpath=/srv/nfs/tqma6
serial#=23000529
set_getcmd=if test "${ipmode}" != static; then setenv getcmd dhcp; setenv autoload yes; else setenv getcmd tftp; setenv autoload no; fi
stderr=serial
stdin=serial
stdout=serial
uboot=u-boot.imx
uboot_size=0x7fe
uboot_start=0x2
uimage=uImage
update_fdt=run fdt_name; if tftp ${fdtimg}; then if itest ${filesize} > 0; then mmc dev ${mmcdev}; mmc rescan; setexpr blkc ${filesize} / 0x200; setexpr blkc ${blkc} + 1; if itest ${blkc} <= ${fdt_size}; then mmc write ${loadaddr} ${fdt_start} ${blkc}; fi; fi; fi; setenv filesize; setenv blkc
update_kernel=run kernel_name; if tftp ${kernel}; then if itest ${filesize} > 0; then mmc dev ${mmcdev}; mmc rescan; setexpr blkc ${filesize} / 0x200; setexpr blkc ${blkc} + 1; if itest ${blkc} <= ${kernel_size}; then mmc write ${loadaddr} ${kernel_start} ${blkc}; fi; fi; fi; setenv filesize; setenv blkc
update_uboot=if tftp ${uboot}; then if itest ${filesize} > 0; then mmc dev ${mmcdev}; mmc rescan; setexpr blkc ${filesize} / 0x200; setexpr blkc ${blkc} + 1; if itest ${blkc} <= ${uboot_size}; then mmc write ${loadaddr} ${uboot_start} ${blkc}; fi; fi; fi; setenv filesize; setenv blkc
usbethaddr=00:d0:93:35:ac:db
zimage=zImage

Environment size: 4027/8188 bytes

0 项奖励
回复
3 回复数

5,910 次查看
dugurlu
Contributor I

yes ı tried that.

0 项奖励
回复

5,910 次查看
diegoadrian
NXP Employee
NXP Employee

Have you tried using the same bootargs as do we have on our reference board? With that configuration you can modify your bootargs, anytime you want it.

Best regards,

Diego.

0 项奖励
回复

5,910 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Have you tried changing the fdt file with the below u-boot command?

u-boot -> env edit fdt_file

edit: <your fdt file> // just change it to your new fdt file

u-boot -> saveenv

Hope this can help you.

Best regards,

Diego.

0 项奖励
回复