How To Verify If Kernel Has Entered into Sleep Mode on MX6DL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How To Verify If Kernel Has Entered into Sleep Mode on MX6DL?

969 次查看
tony_l_cai
Contributor III

Hi,all

     On MX6DL, how to verify if kernel has entered into sleep mode? and another question,I have set VSTBY bit on u-boot,but when system is powered up, why PMIC_STBY_REQ is low? and when I press the pwr key, log is as blow:

request_suspend_state: wakeup (3->0) at 3969200866476 (1970-01-19 21:52:43.407821141 UTC)

request_suspend_state: sleep (0->3) at 3979655170811 (1970-01-19 21:52:53.862126475 UTC)

Whatever the transition from wakeup to sleep or from sleep to wakeup, the PMIC_STBY_REQ is low,why ?

3Q~

标签 (3)
0 项奖励
回复
1 回复

886 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

one can measure board current using

AN4509 i.MX 6Dual/6Quad Power Consumption Measurement

Uboot does not use low power modes, so PMIC_STBY_REQ

is not used.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复