High Assurance Boot Certificate Validity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

High Assurance Boot Certificate Validity

ソリューションへジャンプ
3,816件の閲覧回数
christopherpres
Contributor III

Hi,

I work on a Freescale i.mx28 and I use High Assurance Boot (HAB).

When creating certificates with the "hab4_pki_tree.sh" script, which is provided with the Code Signing Tool, I can enter a certificate validity duration of max. 20 years.

What happens after 20 year? Does the i.mx28 not boot anymore? Am I not able to sign software anymore? Or do I have to add new CSF and IMG certificates to sign software with them?

My questions are: Who checks the certificate duration and when? Which certificates have a limited duration (I assume the root-certificate has unlimited duration)?

Best regards,

Chris

1 解決策
3,128件の閲覧回数
rodz
Contributor III

Hi Chris,

Currently, if the validity period of the certificate expires nothing will happen.  The ROM/HAB does not enforce certificate validity periods and the Code Signing Tool will still allow code to be signed.  The intent is to enforce the cert validity periods with the code signing tool.  However, feature has not yet been added and is planned as an update to the code signing tool.

Regards,

-Rod


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,129件の閲覧回数
rodz
Contributor III

Hi Chris,

Currently, if the validity period of the certificate expires nothing will happen.  The ROM/HAB does not enforce certificate validity periods and the Code Signing Tool will still allow code to be signed.  The intent is to enforce the cert validity periods with the code signing tool.  However, feature has not yet been added and is planned as an update to the code signing tool.

Regards,

-Rod


0 件の賞賛
返信
3,128件の閲覧回数
gurukottur
Contributor I

Hi Rod,

Any update on the certificate expiry and certificate revocation and if the fuses can be revoked?

Regards,

Guru

0 件の賞賛
返信