Hibernating Linux 3.0.35 on IMX6Q SABRE AI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hibernating Linux 3.0.35 on IMX6Q SABRE AI

跳至解决方案
2,210 次查看
shyamjithkv
Contributor III

Hi,

I am working on to implement hibernation (Suspend to disc) on an IMX6Q (SABRE AI EVK) with a 3.0.35 kernel,

I had gone through many patches and links in the web, but couldn't get any right thread to follow.

Can anyone suggest the best way to go ? Any help would be appreciated.

Best regards

shyamjith

标签 (2)
0 项奖励
回复
1 解答
1,967 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shyamjith

hibernation is not supported on  IMX6 linux, there are some example

for other processors, one can try to port them

http://www.gossamer-threads.com/lists/linux/kernel/1882614

http://elinux.org/images/0/0c/Slides.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,968 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shyamjith

hibernation is not supported on  IMX6 linux, there are some example

for other processors, one can try to port them

http://www.gossamer-threads.com/lists/linux/kernel/1882614

http://elinux.org/images/0/0c/Slides.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,967 次查看
shyamjithkv
Contributor III

Hi igor,

That was really helpful,Thank you very much for your time.

Regards,

shyamjith

0 项奖励
回复