Hi, not able to open the link http://git.nxp.com/git/(Source code for imx6 linux)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, not able to open the link http://git.nxp.com/git/(Source code for imx6 linux)

1,368 Views
rajathkumardiva
Contributor II

I am not able to open the source code for imx6 solo source code (linux).i.MX 6 Series Software and Development Tool|NXP . Is this an issue with NXP server ?

Could you please come with a solution download source code for i.mx6 solo linux version.

We are getting below error:

The following error was encountered while trying to retrieve the URL: http://git.nxp.com/git/

Unable to determine IP address from host name git.nxp.com

The DNS server returned:

Name Error: The domain name does not exist.
Labels (1)
0 Kudos
Reply
1 Reply

1,249 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, the source code link is not correct. Really the Linux source codes

should be loaded via git. Please refer to "i.MX_Yocto_Project_User's_Guide.pdf"

in documentation hoe to do it.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply