Hi, not able to open the link http://git.nxp.com/git/(Source code for imx6 linux)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, not able to open the link http://git.nxp.com/git/(Source code for imx6 linux)

1,387件の閲覧回数
rajathkumardiva
Contributor II

I am not able to open the source code for imx6 solo source code (linux).i.MX 6 Series Software and Development Tool|NXP . Is this an issue with NXP server ?

Could you please come with a solution download source code for i.mx6 solo linux version.

We are getting below error:

The following error was encountered while trying to retrieve the URL: http://git.nxp.com/git/

Unable to determine IP address from host name git.nxp.com

The DNS server returned:

Name Error: The domain name does not exist.
ラベル(1)
0 件の賞賛
返信
1 返信

1,268件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, the source code link is not correct. Really the Linux source codes

should be loaded via git. Please refer to "i.MX_Yocto_Project_User's_Guide.pdf"

in documentation hoe to do it.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信