Help identifying an imx6d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help identifying an imx6d

1,568 Views
richogrady
Contributor II

We have a batch of imx6d Rev 1.3 that we are having trouble identifying.  These are automotive grade marked on top as MCIMX6D6AVT08AD.  This is what we ordered, this is what we wanted.  

The ANATOP_DIGPROG register reads 0x630005.  So far, so good.  If we read the SCU_CONFIG register it reads as 0x5503.  The '3' indicates a quad core.  Did we receive parts that were marked incorrectly?

On a batch of imx6d Rev 1.2 parts we read SCU_CONFIG as 0x5501.  In this case, the '1' indicates a dual core part (as expected).

3 Replies

1,459 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Is the problem still takes place ?

If so, please create request (ticket)

Sales and Support|NXP 

Regards,

Yuri.

0 Kudos
Reply

1,459 Views
richogrady
Contributor II

Yuri,

We returned these parts to our supplier as we feel they may be counterfeit.

1,459 Views
b36401
NXP Employee
NXP Employee

You can boot Linux and run "cat /proc/cpuinfo" command.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply