Help Flashing Fresh Android image to Riotboard uboot using Linux Mint as the enviroment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help Flashing Fresh Android image to Riotboard uboot using Linux Mint as the enviroment

1,617 次查看
keithkaaos
Contributor I

hello all i am in desperate need of some emergency help. i use my riotboard for 90% of my online and technical work. And yesterday i was trying to adjust the screen resolution (which i have been wanting it to work on  a small hdmi for a while now) and somehow while in uboot i screwed something up and i need to put a fresh image on there. My original image was done using windows but i dont have access to that machine and i need to be able to flash on linux and i can only find directions online for windows and the directions i do find for linux are for flashing ubuntu not android.  i need a mfgtool for linux which ive been seeing is apperently out there somewhere, i just dont have the ability to produce. if i could only find step by step directioins for flashing android KK or LP to the board and NOT a  SD card i need it to be on the actual board. someone please help me. i have a uart cable so i think im set to go i just need the directions. someone please!!! help!!! thank you

0 项奖励
回复
1 回复

1,495 次查看
b36401
NXP Employee
NXP Employee

You can burn SD card partitions manually with Linux dd utility.
Please refer chapter 5.1.1 "Storage partitions" of AndroidTM User's Guide for the details.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复