Hello everyone, there is an error while building Bitbake imx image core. Please seek help!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hello everyone, there is an error while building Bitbake imx image core. Please seek help!!

1,245 次查看
Allenwowo
Contributor I

this log!

allen@localhost:~/Imx8_Linux/imx-yocto-bsp/build_wayland$ bitbake imx-image-core
NOTE: Reconnecting to bitbake server...
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###################################################################################################################################################| Time: 0:00:02
Loaded 5712 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8qm-mek"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:02eacd385eca7aa9cf25aaaa61427aa9c126e0bc"
meta-oe
meta-multimedia
meta-python = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-freescale = "HEAD:41b923e59e048b9b2942ff737a4ddac386954c62"
meta-freescale-3rdparty = "HEAD:8b61684f0b1ba8bacdf3a69d993445e9791d4932"
meta-freescale-distro = "HEAD:158cc55b6ee30d09957b380859dba52c0f6af68d"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:ae04eecd48e557437ec90366795b8cf202d0ce14"
meta-nxp-demo-experience = "HEAD:5c0d6796620b911f7445da5537a6d71cb9764ab4"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:96311d23e51ddd76cfa73a8bbd65b13c82ab5f7d"
meta-arm
meta-arm-toolchain = "HEAD:8aa8a1f17f5b64bc691544f989f04fc83df98adb"
meta-chromium = "HEAD:dc31889c0899971def535dc1c040edf18bc16691"
meta-clang = "HEAD:66414c17ae60e489bef9a97031323e92c247fbe1"
meta-gnome
meta-networking
meta-filesystems = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:1a547c0aa0d75c4143cbb66de6e653d51cdc8bda"

WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile is tainted from a forced run | ETA: 0:00:00
WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile_kernelmodules is tainted from a forced run
WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_deploy is tainted from a forced run
Sstate summary: Wanted 2097 Local 0 Mirrors 0 Missed 2097 Current 1986 (0% match, 48% complete)########################################################## | ETA: 0:00:00
Initialising tasks: 100% |##############################################################################################################################################| Time: 0:00:04
NOTE: Executing Tasks
ERROR: slang-2.3.3-r0 do_compile: oe_runmake failed
ERROR: slang-2.3.3-r0 do_compile: ExecutionError('/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/temp/run.do_compile.35669', 1, None, None)
ERROR: Logfile of failure stored in: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/temp/log.do_compile.35669
Log data follows:
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'bit-64', 'arm-common', 'arm-64', 'common-linux', 'common-glibc', 'aarch64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_compile
| NOTE: make RPATH=
| cd src; make elf
| make[1]: Entering directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src'
| make[1]: Nothing to be done for 'elf'.
| make[1]: Leaving directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src'
| cd slsh; make all
| make[1]: Entering directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/slsh'
| aarch64-poky-linux-gcc -march=armv8-a+crc+crypto -mbranch-protection=standard -fstack-protector-strong -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot objs/slsh.o objs/readline.o -o objs/slsh_exe -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fcanon-prefix-map -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native= -Wl,-z,relro,-z,now -Wl,-export-dynamic -L/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs -lslang -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fcanon-prefix-map -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native= -Wl,-z,relro,-z,now -ldl -lm
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `get_screen_size':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:824:(.text+0x2c): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /usr/src/debug/slang/2.3.3/slsh/readline.c:825:(.text+0x40): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `rline_call_update_hook':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:918:(.text+0x724): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `call_simple_update_cb':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:850:(.text+0x7c8): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `get_input_line':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:490:(.text+0xcd8): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_double'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_pop_uint64'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_bin_op'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_register_types'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_double'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_long_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_uint'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_pop_int64'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_uchar'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_Inf'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLset_double_format'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_float'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLget_double_format'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_uint'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_float'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_char'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_strlen_type'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_get_precedence'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_long_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_NaN'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_char'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_typecast'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_Arith_Types'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_uchar'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_strlen_type'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLformat_as_binary'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLarith_get_to_double_fun'
| collect2: error: ld returned 1 exit status
| make[1]: Leaving directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/slsh'
| make[1]: *** [Makefile:93: objs/slsh_exe] Error 1
| make: *** [Makefile:59: elf] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/allen/Imx8_Linux/imx-yocto-bsp/sources/poky/meta/recipes-extended/slang/slang_2.3.3.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2975 tasks of which 2970 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/allen/Imx8_Linux/imx-yocto-bsp/sources/poky/meta/recipes-extended/slang/slang_2.3.3.bb:do_compile
Summary: There were 4 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.

0 项奖励
回复
2 回复数

1,208 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

The BSP mostly tested on host 22.04. Suggest to not use 24.04

And the CPU cores and memory size should be having a scale of 1 on 4.

 

Regards

Harvey

1,186 次查看
Allenwowo
Contributor I

ok

0 项奖励
回复