Hello everyone, there is an error while building Bitbake imx image core. Please seek help!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello everyone, there is an error while building Bitbake imx image core. Please seek help!!

1,780件の閲覧回数
Allenwowo
Contributor I

this log!

allen@localhost:~/Imx8_Linux/imx-yocto-bsp/build_wayland$ bitbake imx-image-core
NOTE: Reconnecting to bitbake server...
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###################################################################################################################################################| Time: 0:00:02
Loaded 5712 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8qm-mek"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:02eacd385eca7aa9cf25aaaa61427aa9c126e0bc"
meta-oe
meta-multimedia
meta-python = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-freescale = "HEAD:41b923e59e048b9b2942ff737a4ddac386954c62"
meta-freescale-3rdparty = "HEAD:8b61684f0b1ba8bacdf3a69d993445e9791d4932"
meta-freescale-distro = "HEAD:158cc55b6ee30d09957b380859dba52c0f6af68d"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:ae04eecd48e557437ec90366795b8cf202d0ce14"
meta-nxp-demo-experience = "HEAD:5c0d6796620b911f7445da5537a6d71cb9764ab4"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:96311d23e51ddd76cfa73a8bbd65b13c82ab5f7d"
meta-arm
meta-arm-toolchain = "HEAD:8aa8a1f17f5b64bc691544f989f04fc83df98adb"
meta-chromium = "HEAD:dc31889c0899971def535dc1c040edf18bc16691"
meta-clang = "HEAD:66414c17ae60e489bef9a97031323e92c247fbe1"
meta-gnome
meta-networking
meta-filesystems = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:1a547c0aa0d75c4143cbb66de6e653d51cdc8bda"

WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile is tainted from a forced run | ETA: 0:00:00
WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile_kernelmodules is tainted from a forced run
WARNING: /home/allen/Imx8_Linux/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_deploy is tainted from a forced run
Sstate summary: Wanted 2097 Local 0 Mirrors 0 Missed 2097 Current 1986 (0% match, 48% complete)########################################################## | ETA: 0:00:00
Initialising tasks: 100% |##############################################################################################################################################| Time: 0:00:04
NOTE: Executing Tasks
ERROR: slang-2.3.3-r0 do_compile: oe_runmake failed
ERROR: slang-2.3.3-r0 do_compile: ExecutionError('/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/temp/run.do_compile.35669', 1, None, None)
ERROR: Logfile of failure stored in: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/temp/log.do_compile.35669
Log data follows:
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'bit-64', 'arm-common', 'arm-64', 'common-linux', 'common-glibc', 'aarch64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_compile
| NOTE: make RPATH=
| cd src; make elf
| make[1]: Entering directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src'
| make[1]: Nothing to be done for 'elf'.
| make[1]: Leaving directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src'
| cd slsh; make all
| make[1]: Entering directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/slsh'
| aarch64-poky-linux-gcc -march=armv8-a+crc+crypto -mbranch-protection=standard -fstack-protector-strong -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot objs/slsh.o objs/readline.o -o objs/slsh_exe -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fcanon-prefix-map -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native= -Wl,-z,relro,-z,now -Wl,-export-dynamic -L/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs -lslang -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fcanon-prefix-map -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3=/usr/src/debug/slang/2.3.3 -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fmacro-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot= -fdebug-prefix-map=/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native= -Wl,-z,relro,-z,now -ldl -lm
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `get_screen_size':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:824:(.text+0x2c): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /usr/src/debug/slang/2.3.3/slsh/readline.c:825:(.text+0x40): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `rline_call_update_hook':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:918:(.text+0x724): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `call_simple_update_cb':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:850:(.text+0x7c8): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: objs/readline.o: in function `get_input_line':
| /usr/src/debug/slang/2.3.3/slsh/readline.c:490:(.text+0xcd8): undefined reference to `SLang_push_int'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_double'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_pop_uint64'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_bin_op'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_register_types'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_double'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_long_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_uint'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_pop_int64'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_uchar'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_Inf'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLset_double_format'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_float'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLget_double_format'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_uint'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_float'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_char'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_strlen_type'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_get_precedence'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_long_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLang_NaN'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_char'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_typecast'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLarith_Arith_Types'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_uchar'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_strlen_type'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_pop_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLang_push_long'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `_pSLformat_as_binary'
| /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.2.0/ld: /home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/src/elfobjs/libslang.so: undefined reference to `SLarith_get_to_double_fun'
| collect2: error: ld returned 1 exit status
| make[1]: Leaving directory '/home/allen/Imx8_Linux/imx-yocto-bsp/build_wayland/tmp/work/armv8a-poky-linux/slang/2.3.3/slang-2.3.3/slsh'
| make[1]: *** [Makefile:93: objs/slsh_exe] Error 1
| make: *** [Makefile:59: elf] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/allen/Imx8_Linux/imx-yocto-bsp/sources/poky/meta/recipes-extended/slang/slang_2.3.3.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2975 tasks of which 2970 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/allen/Imx8_Linux/imx-yocto-bsp/sources/poky/meta/recipes-extended/slang/slang_2.3.3.bb:do_compile
Summary: There were 4 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.

0 件の賞賛
返信
2 返答(返信)

1,743件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

The BSP mostly tested on host 22.04. Suggest to not use 24.04

And the CPU cores and memory size should be having a scale of 1 on 4.

 

Regards

Harvey

1,721件の閲覧回数
Allenwowo
Contributor I

ok

0 件の賞賛
返信