Hello World application for iMX6UL device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello World application for iMX6UL device

2,465 Views
cyriacdevasia
Contributor I

I am new to the embedded linux world.

I have a new iMX6ULEVK board and it boots up fine with the pre-loaded image as mentioned in the Quick Start guide. I am using TeraTerm and the board is connected to a serial port.

The pre-loaded image doesn't seem to have the GNU compiler or other Linux tools. How do I go about adding these? Is there an app note on how to develop and run a basic "Hello World" application on the iMX6UL device?

Labels (1)
0 Kudos
Reply
1 Reply

2,130 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cyriac

one can follow common linux hello world examples:

Hello World program for the i.MX6 Solox on Sabresd board running Linux. 

http://www.variwiki.com/index.php?title=VAR-SOM-MX6_Hello_World

may be useful to check documentation on software resources link

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply