Having trouble with network connectivity when using multiple Ethernet interfaces in NXP i.MX 8M plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having trouble with network connectivity when using multiple Ethernet interfaces in NXP i.MX 8M plus

2,526件の閲覧回数
Kiruthik-15
Contributor I

Hello Everyone,

I'm experiencing network connectivity issue , I'm unable to ping when using multiple Ethernet interfaces .

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,415件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @Kiruthik-15 

I have not do any change on my site, just use the default BSP code.

Because you sail "This occurs despite the laptop being connected to the internet via Wi-Fi" you should check your vpn.

B.R

 

 

 

0 件の賞賛
返信

2,454件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @Kiruthik-15 

i try your issue on my site, there is no problem occur on my site. Have you check if your network can access 8.8.8.8? 

pengyong_zhang_0-1725502812387.png

 

B.R 

0 件の賞賛
返信

2,445件の閲覧回数
Kiruthik-15
Contributor I

Hi Pengyong_zhang,

May I know what steps you have followed and if it's possible may i know which image you have used for the sdk.

 

B.R

0 件の賞賛
返信

2,436件の閲覧回数
Kiruthik-15
Contributor I
I think its based on routing preference
when the route eth0 is initially up then this issue is present .
Could you check , from my understanding i think this is due to routing (not sure) , please correct me if im wrong
0 件の賞賛
返信

2,505件の閲覧回数
Kiruthik-15
Contributor I
In the EVK , the ETH0 is able to ping camera and ETH1 is able to ping laptop . But However, when I attempt to ping an external IP address (e.g., 8.8.8.8) from the NXP i.MX MPlus Board, the request times out. This occurs despite the laptop being connected to the internet via Wi-Fi.
0 件の賞賛
返信