Has errata fixed in enhanced EPDC of i.MX6SLL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has errata fixed in enhanced EPDC of i.MX6SLL?

Jump to solution
1,102 Views
torus1000
Contributor V

Hi, 

I compared two errata(IMX6SLLCE.pdf and IMX6SLCE.pdf) then found known EDDC errata ERR005313 disappeared.
I guess errata was fixed but I couldn't find any descriptions in "i.MX 6SLL Migration Guide: AN11988.pdf".

Has the errata ERR005313 been already fixed?

If someone know it, please let me know.

ERR005313 EPDC: Incorrect data fetched when the buffer update width is 2048 pixels or greater

Description:
When sending an image update to a high resolution panel with an image buffer width ≥ 2048 pixels,
the EPDC module fetches incorrect data because an internal address register is incorrectly
truncated.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
937 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Torus1000,

I confirmed that this erratum was fixed since i.MX6SL and it is also fixed on the i.MX6SLL.

I hope this helps!

Regards,

View solution in original post

0 Kudos
Reply
1 Reply
938 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Torus1000,

I confirmed that this erratum was fixed since i.MX6SL and it is also fixed on the i.MX6SLL.

I hope this helps!

Regards,

0 Kudos
Reply