Harpoon without Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Harpoon without Linux

2,317件の閲覧回数
simmania
Contributor IV

Hi,

When I look at the pictures about Harpoon it seems that Both Linux and other RTOS modules are running on top of Jailhouse Hypervisor. It also says:

"Enables a choice of RTOS’s to run within Jailhouse hypervisor environment on the Arm® Cortex®-A cores of NXP MPU’s."

So this implies Harpoon can be used without Linux. Is that correct?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,262件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Simmania:

From the Harpoon User's Guide: Linux is needed

danielchen_0-1746582449571.png

 

 

Regards

Daniel

0 件の賞賛
返信

2,251件の閲覧回数
simmania
Contributor IV

This text does not say that Linux is required. It says that both Linux and an RTOS can run in parallel on the Harpoon environment. That does not mean that Linux is mandatory.

0 件の賞賛
返信

2,150件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Thanks, but the doc says the system starts on Linux and the Jailhouse hypervisor partitions the hardware to run both Linux and the guest RTOS in parallel.

 

danielchen_1-1747703720860.png

 

0 件の賞賛
返信