Hardware decoding video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware decoding video

1,492 Views
romannazar
Contributor I

What libraries can be used for HARDWARE decoding video on IMX6? And where to find them?

0 Kudos
Reply
1 Reply

1,355 Views
igorpadykov
NXP Employee
NXP Employee

Hi Roman

one needs to install codecs:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

L3.0.35_4.1.0_MM_CODECS : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux Multimedia Codecs Sources.

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

L3.0.35_4.1.0_LINUX_MMDOCS

L3.0.35_4.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply