Hardware Cryptography in FreeRTOS (CAAM)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware Cryptography in FreeRTOS (CAAM)

1,011 Views
timholland
Contributor I

We want to use the CAAM device from freeRTOS.

We are using an iMX7D and currently we have Sabre SD boards for prototyping.

Has anybody implemented a device driver or interface to the CAAM for hardware cryptography in freeRTOS?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

875 Views
art
NXP Employee
NXP Employee

No, there is no CAAM driver for the i.MX7D M4 core FreeRTOS BSP has been implemented so far.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply