HY4635 touch controller not responding properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HY4635 touch controller not responding properly

3,312 Views
karthikssk
Contributor I

Hi,

I am using a 7" LCD (800*480)display(RGB interface) with cap touch (I2C interface) and the touch controller used is HY4635 and IMX6 SOLO processor is used. So the response of the touch is not very accurate and when the values are read in terminal window most of the time it shows wrong (X,Y) values like out of bound. 

Only some times there is the response . we cannot  do the drag operation but once in a while just single touch will respond that to very slowly . 

Can anyone please suggest whats the issue?

Any driver changes that need to be done ?

Tags (1)
0 Kudos
Reply
1 Reply

2,383 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karthik

one can test with linux driver provided by HY4635 vendor

http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip 

and try to calibrate using guidelines on

Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply