HID as wakeup device in Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HID as wakeup device in Android

2,413 Views
sandheepkumar
Contributor I

Hi All,

I am currently working in a custom imx6 sabresd board running on Android Kitkat 4.4.2 with linux kernel 3.0.35. I have interfaced an eGalax USB touchscreen device with my imx6 development kit. The touchscreen works under HID multitouch driver. I would like to configure the Touchscreen to wakeup the imx6 system from the suspend state. Can anyone provide me some information regarding this implementation?

Regards,

Sandheep

0 Kudos
Reply
1 Reply

2,003 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandheep

for examples of usb wake-up one can look at sect.34.3.3 WakeUp

Events Supported by USB attached Linux Manual.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply