HID as wakeup device in Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HID as wakeup device in Android

2,662件の閲覧回数
sandheepkumar
Contributor I

Hi All,

I am currently working in a custom imx6 sabresd board running on Android Kitkat 4.4.2 with linux kernel 3.0.35. I have interfaced an eGalax USB touchscreen device with my imx6 development kit. The touchscreen works under HID multitouch driver. I would like to configure the Touchscreen to wakeup the imx6 system from the suspend state. Can anyone provide me some information regarding this implementation?

Regards,

Sandheep

タグ(5)
0 件の賞賛
返信
1 返信

2,252件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sandheep

for examples of usb wake-up one can look at sect.34.3.3 WakeUp

Events Supported by USB attached Linux Manual.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信