HDMI resolution effected when we enabled LVDS display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI resolution effected when we enabled LVDS display

1,170 Views
shiva141
Contributor II

Hi,

IMX8MP Android 13 we have build the bsp based on user guide.

 

We were able to see full resolution on HDMI ,while HDMI was only enabled.


When we enabled LVDS support in the BSP, we observed  that the LVDS resolution had an impact on the HDMI resolution.

 

When LVDS is enabled in the Android BSP, is it possible to attain full resolution on HDMI?



IMX8MPLUS #Andorid13

 

 

0 Kudos
Reply
2 Replies

1,152 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Are you using lvds-panel dtbo.image?

To test LVDS panel display, execute the tool with -d lvds-panel. MIPI-to-HDMI and physical HDMI
are also supported in this condition



Best Regards
Zhiming

0 Kudos
Reply

1,142 Views
shiva141
Contributor II
Hi

- Yes , we are using -d lvds-panel
- Both HDMI and LVDS are connected to target

sudo ./imx-sdcard-partition.sh -d lvds-panel -f imx8mp -c 28 /dev/sdc
0 Kudos
Reply