HDMI resolution effected when we enabled LVDS display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI resolution effected when we enabled LVDS display

1,177件の閲覧回数
shiva141
Contributor II

Hi,

IMX8MP Android 13 we have build the bsp based on user guide.

 

We were able to see full resolution on HDMI ,while HDMI was only enabled.


When we enabled LVDS support in the BSP, we observed  that the LVDS resolution had an impact on the HDMI resolution.

 

When LVDS is enabled in the Android BSP, is it possible to attain full resolution on HDMI?



IMX8MPLUS #Andorid13

 

 

0 件の賞賛
返信
2 返答(返信)

1,159件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Are you using lvds-panel dtbo.image?

To test LVDS panel display, execute the tool with -d lvds-panel. MIPI-to-HDMI and physical HDMI
are also supported in this condition



Best Regards
Zhiming

0 件の賞賛
返信

1,149件の閲覧回数
shiva141
Contributor II
Hi

- Yes , we are using -d lvds-panel
- Both HDMI and LVDS are connected to target

sudo ./imx-sdcard-partition.sh -d lvds-panel -f imx8mp -c 28 /dev/sdc
0 件の賞賛
返信