HDMI reference clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI reference clock

1,875件の閲覧回数
ajaykumar_d
Contributor II

Hi

For HDMI in i.MX 8M there is two Reference clock input (crystal at XTALI/O at pin no V25/V24 and Differential HDMI_REFCLK_N/P at Pin No R1/R2), both are used for HDMI PHY. are both clocks required or anyone clock is sufficient?

ラベル(1)
タグ(1)
1 返信

1,668件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi  ajay,

That clock feed a lot of modules running to 24 Mhz. so ideally the MX8m can run HDMI with only XTLAI_27MHz and not use an external REFCLK. But it is not verified yet

Regards