HDMI phy_int_stat value when cable is plugged

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HDMI phy_int_stat value when cable is plugged

跳至解决方案
2,415 次查看
TKayO
Contributor III

Hello, 

my previous question about HDMI of i.MX6

It's about the HDMI working status is different,

1) when my board boot up with HDMI monitor connected (hdmi is work with no problem)

2) HDMI monitor connected after boot up  (not working)

https://community.nxp.com/t5/i-MX-Processors/imx6-HDMI-working-status-differed-by-cable-plugging/m-p...

 

And I enabled mxc_hdmi debug messages, and found differences.

 

Log of nicely working hdmi (cable plugged when powered up)

[ 93.136869] mxc_hdmi 20e0000.hdmi_video: Hotplug interrupt received
[ 93.157514] mxc_hdmi 20e0000.hdmi_video: phy_int_stat=0x3d, phy_int_pol=0x2
[ 93.157522] mxc_hdmi 20e0000.hdmi_video: EVENT=plugin
[ 93.157532] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected
[ 93.157540] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid
[ 93.157760] mxc_hdmi 20e0000.hdmi_video: read failed
[ 93.157768] mxc_hdmi 20e0000.hdmi_video: Read EDID again
[ 93.377540] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid
[ 93.377763] mxc_hdmi 20e0000.hdmi_video: read failed
[ 93.377772] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_default_modelist
[ 93.377779] mxc_hdmi 20e0000.hdmi_video: create default modelist
[ 93.382527] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode
[ 93.382550] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode: Video mode same as previous
[ 93.382557] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup
[ 93.382576] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed
[ 93.382596] hdmi_disable_overflow_interrupts
[ 93.382604] mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=16
[ 93.382611] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer
[ 93.382619] mxc_hdmi 20e0000.hdmi_video: final pixclk = 148500000
[ 93.382626] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit
[ 93.382633] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[ 93.382638] hdmi_enable_overflow_interrupts
[ 93.382647] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[ 93.394689] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[ 93.406728] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path
[ 93.406738] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode
[ 93.406751] mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk
[ 93.406758] mxc_hdmi 20e0000.hdmi_video: set up AVI frame
[ 93.406781] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit\x0a
[ 93.406789] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected exit

 

Log of no display on hdmi monitor (power up without cable, after boot, cable plugged)

 

[ 86.152376] mxc_hdmi 20e0000.hdmi_video: Hotplug interrupt received
[ 86.177489] mxc_hdmi 20e0000.hdmi_video: phy_int_stat=0x1, phy_int_pol=0x2
[ 86.177498] mxc_hdmi 20e0000.hdmi_video: EVENT=plugin
[ 86.177509] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected
[ 86.177518] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid
[ 86.177939] mxc_hdmi 20e0000.hdmi_video: read failed
[ 86.177949] mxc_hdmi 20e0000.hdmi_video: Read EDID again
[ 86.397465] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid
[ 86.397675] mxc_hdmi 20e0000.hdmi_video: read failed
[ 86.397684] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_default_modelist
[ 86.397692] mxc_hdmi 20e0000.hdmi_video: create default modelist
[ 86.402446] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode
[ 86.402469] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode: New video mode
[ 86.402477] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode_to_vga_dvi
[ 86.402482] hdmi_disable_overflow_interrupts
[ 86.402493] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb
[ 86.402500] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_disable
[ 86.402548] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE
[ 86.402558] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup
[ 86.402574] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed
[ 86.402578] hdmi_disable_overflow_interrupts
[ 86.402584] mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=0
[ 86.402591] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer
[ 86.402597] mxc_hdmi 20e0000.hdmi_video: final pixclk = 24780000
[ 86.402603] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit
[ 86.402613] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[ 86.402618] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path
[ 86.402626] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode
[ 86.402634] mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk
[ 86.402640] mxc_hdmi 20e0000.hdmi_video: set up AVI frame
[ 86.402662] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit\x0a
[ 86.402670] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb exit
[ 86.402686] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb
[ 86.402692] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_disable
[ 86.402727] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE
[ 86.402733] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup
[ 86.402747] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed
[ 86.402764] hdmi_disable_overflow_interrupts
[ 86.402770] mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=16
[ 86.402776] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer
[ 86.402784] mxc_hdmi 20e0000.hdmi_video: final pixclk = 148500000
[ 86.402790] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit
[ 86.402795] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[ 86.402801] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path
[ 86.402809] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode
[ 86.402820] mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk
[ 86.402827] mxc_hdmi 20e0000.hdmi_video: set up AVI frame
[ 86.402850] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit\x0a
[ 86.402858] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb exit
[ 86.402865] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected exit

 

Any idea of what cause these differences?

Thank you.

 

ps.

mxc_hdmi_phy_init() function in module "KERNEL/drivers/video/fbdev/mxc/mxc_hdmi.c"

seems the cause of this situation.

 

    if (!hdmi->fb_reg || !hdmi->cable_plugin
            || (hdmi->blank != FB_BLANK_UNBLANK))
        return;

 

above condition returned with "hdmi->blank != FB_BLANK_UNBLANK" is true.

标签 (1)
0 项奖励
回复
1 解答
2,400 次查看
igorpadykov
NXP Employee
NXP Employee

Hi WOOSEOK

 

please try to reproduce issue on NXP Sabre SD reference board with linux releases described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,401 次查看
igorpadykov
NXP Employee
NXP Employee

Hi WOOSEOK

 

please try to reproduce issue on NXP Sabre SD reference board with linux releases described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 项奖励
回复
2,389 次查看
TKayO
Contributor III

Thank you for your concern

and sorry for my frequent questions.

it was a hardware problem.  there was no pull-up register for the HPD pin.

 

0 项奖励
回复