HDMI custom resolution and clock setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI custom resolution and clock setting

4,469件の閲覧回数
lsg5131420
Contributor III

Hi

I want to add support for 1280*800 and 1366*768 resolution with hdmi display on imx8mq. By reading the code,I found the pixel clock 85.5M(1366*768) and 71.1M(1280*800)  was not  supported. i am afraid  i shouled modify table 8(t28hpc_hdmitx_clock_control_table_pixel_out[]) and table 9(t28hpc_hdmitx_pll_tuning_table_pixel_out[]) to support 85.5M and 71.M. and I have read the IMX8MDQLQRM datesheet. and it does not describe about this. How can I to config these tables?

BR

Liu

0 件の賞賛
返信
7 返答(返信)

4,323件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The resolutions 3840x2160,1920x1080, 1280x720, 720x480 are support in our default BSP. For the other resolutions work you need to change the clocks accordingly to the display requirements.

Here I found the patch based on the Linux 4.14.78-1.0.0_ga version BSP. Hope can do help for you.

0 件の賞賛
返信

4,323件の閲覧回数
lsg5131420
Contributor III

Hi Rita

Thanks for your reply. I use the BSP version is Linux 4.14.98. I found my quesiton  is answered on HDMI DRM custom resolution and clock frequency . They use  HDMI - pixel clock calculation tools to generate coustom hdmi pixel clock. But I can not download the tools because of no authorization. Please send the tools to me, if that is convinent.

Thanks very much.

Best regards

Shiguang Liu

0 件の賞賛
返信

4,323件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I have email to you, please check.

0 件の賞賛
返信

4,323件の閲覧回数
lsg5131420
Contributor III

Hi Rita

Thank you very much. It is useful to me.

Best regards.

Shiguang Liu

0 件の賞賛
返信

4,323件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome~~

0 件の賞賛
返信

4,323件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Shiguang,

OK, I will do confirm it and then give you reply.

Have a nice day

Best regards

Rita

0 件の賞賛
返信

4,323件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 件の賞賛
返信