HDMI audio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI audio

3,815 Views
Poo
Contributor II

Hi All,

I'm working on a board with imx51 processor and i have my HDMI interface up and  working. Now i need to send audio over HDMI and play audio on a HDMI compatible TV.

Can someone point out what are the drivers to be enabled to achieve this, any additional information regarding this is highly appreciated.

Thank You

Poo

Tags (1)
0 Kudos
Reply
5 Replies

3,323 Views
daiane_angolini
NXP Employee
NXP Employee

I know there is some work on HDMI audio for iMX53, I´m not sure what are and are not supported, but I believe it source code can guide you someway.

Please, take a look on:

http://opensource.freescale.com/git?p=imx/linux-2.6-imx.git;a=commit;h=2f161b93baebacc99f5a454f4a58d...

http://opensource.freescale.com/git?p=imx/linux-2.6-imx.git;a=commit;h=9ea5b20802d0246bf8de3a8d915ed...

0 Kudos
Reply

3,323 Views
Poo
Contributor II

Hi Kevin,

Thank you for responding.

I'm using SiI9022A hdmi transmitter.


kevin chen said:

which hdmi phy chip on your imx51 board?

0 Kudos
Reply

3,323 Views
superlibj8301
Contributor I

Hi Po P,

I'm also using the Sil9022A HDMI transmitter on LS1, could you tell me where could i find your Sil9022A HDMI driver please ?

Thanks,

Best Regards,

0 Kudos
Reply

3,323 Views
saurabh206
Senior Contributor III

Hi

Superlib

Contact Silicon Image for the SII9022A driver.

Regards,

Saurabh

0 Kudos
Reply

3,323 Views
KevinChen_ng
Contributor I

which hdmi phy chip on your imx51 board?

0 Kudos
Reply