HDMI audio not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI audio not working

1,732 Views
priyaprasad
Contributor I

We are using Sabrelite  board (Boundary device) (imx6Q) ,  When we are testing it, we could find following things:

1. On HDMI audio is not coming with Ubuntu trusty , xenial and Android 7 releases of Boundary devices.

Please help in resolving this issue.

Regards

Priya

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,644 Views
igorpadykov
NXP Employee
NXP Employee

Hi Priya

HDMI audio playback depends on HDMI pixel clock. as described in

sect.15.2.5 Audio attached Linux Manual, so one can check if clocks are appropriate.

Also Sabrelite is supported by third party BD and this may be posted on meta-fsl-arm mailing list,

so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply