HDMI audio not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HDMI audio not working

1,708 次查看
priyaprasad
Contributor I

We are using Sabrelite  board (Boundary device) (imx6Q) ,  When we are testing it, we could find following things:

1. On HDMI audio is not coming with Ubuntu trusty , xenial and Android 7 releases of Boundary devices.

Please help in resolving this issue.

Regards

Priya

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,620 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Priya

HDMI audio playback depends on HDMI pixel clock. as described in

sect.15.2.5 Audio attached Linux Manual, so one can check if clocks are appropriate.

Also Sabrelite is supported by third party BD and this may be posted on meta-fsl-arm mailing list,

so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复