HDMI audio not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI audio not working

1,739件の閲覧回数
priyaprasad
Contributor I

We are using Sabrelite  board (Boundary device) (imx6Q) ,  When we are testing it, we could find following things:

1. On HDMI audio is not coming with Ubuntu trusty , xenial and Android 7 releases of Boundary devices.

Please help in resolving this issue.

Regards

Priya

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,651件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Priya

HDMI audio playback depends on HDMI pixel clock. as described in

sect.15.2.5 Audio attached Linux Manual, so one can check if clocks are appropriate.

Also Sabrelite is supported by third party BD and this may be posted on meta-fsl-arm mailing list,

so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信