HDMI - Resolution Isuue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI - Resolution Isuue

1,798 Views
rizwan_s
Contributor II

Hi,

I am working on imx6Q board with linux yocto 3.14.38.

Please clarify the following observations.

1.In Uboot, I have set 1920x1080@60 and connected the 1920x1080 hdmi monitor, then the image looks proper and fbset shows the proper values for resolution as 1920x1080.

If i connect other lower resolution monitor (1280x720) ,The image looks like 640x480 and when verified with fbset, it shows 640x480

2.If the resolution is changed to 1280x720@60 during uboot, The image looks proper on 1280x720 Monitor.

If the same is connected to 1920x1080 monitor.It shows big icons and fbset shows the resolution as 640x480@60

How does the resolution differs on HDMI monitor.Is it due to HDMI monitor settings or due to settings in Linux BSP.

Please clarify

Thanks and Regards

Rizwan Syed

Labels (5)
0 Kudos
Reply
1 Reply

1,534 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

please look at splashscreen patches on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

seems 640x480 is default resolution so it is used if any problem happens.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply