HDMI HOT PLUG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI HOT PLUG

2,150件の閲覧回数
avenkatramani
Contributor III

HI 

I am trying to detect the hot-plug option in imx6. i can able detect the plugin and plug-out on cable_status on ly on reboot. i checked the HW for plug in/out voltage ranges also.

the hot-plug functionality not working. 

can any point the correct dts configuration for the hot-plug pin.

Thanks.

タグ(1)
0 件の賞賛
返信
1 返信

2,052件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunkumar 

it is working on i.MX6Q Sabre boards:

iMX6Q-SABRE-SDB-DESIGNFILES

https://www.nxp.com/webapp/Download?colCode=iMX6Q-SABRE-SDB-DESIGNFILES&appType=license 

Linux L4.14.98_2.0.0 Documentation

some hdmi hot plug issues are well described on

https://boundarydevices.com/dvi-support-on-i-mx6-boards/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信