HDMI Dispaly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI Dispaly

2,361件の閲覧回数
prasads
Contributor I

Hi,

I am using imx6 sabre auto development board.i used a HDMI converter cable by connecting  to VGA monitor for the display.But i am not able to get any display in my VGA monitor.

I used the environment variables for HDM to set in commanline arguments:

setenv bootargs 'console=ttymxc3,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc3 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.serialno=112029d4df666d04'

Please find the hdmi logs below:

booti mmc1

kernel   @ 14008000 (6821344)

ramdisk  @ 15000000 (726561)

fdt      @ 14f00000 (50597)

kernel cmdline:

        use boot.img command line:

        console=ttymxc3,115200 androidboot.console=ttymxc3 init=/init video=mxcfb0:dev=hdmi,640x480M@60,bpp=32 video=mxcfb1:off video=mxcfb2:o4

   Using Device Tree in place at 14f00000, end 14f0f5a4

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 3.10.53 (khirod@root-T430) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #48 SMP PREEMPT Wed Feb 3 03:00:03 IST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Automotive Board

cma: CMA: reserved 384 MiB at 66000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @82008000 s9728 r8192 d14848 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 520464

Kernel command line: console=ttymxc3,115200 androidboot.console=ttymxc3 init=/init video=mxcfb0:dev=hdmi,640x480M@60,bpp=32 video=mxcfb1:off v4

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)

Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)

Memory: 1983MB 64MB = 2047MB total

Memory: 1666872k/1666872k available, 430280k reserved, 269312K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)

    lowmem  : 0x80000000 - 0xef800000   (1784 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80e7b484   (14798 kB)

      .init : 0x80e7c000 - 0x80ed0600   ( 338 kB)

      .data : 0x80ed2000 - 0x80f56000   ( 528 kB)

       .bss : 0x80f56000 - 0x80feacf8   ( 596 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x807e31d0 - 0x807e3228

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1100 mV

vdd3p0: 2625 <--> 3400 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2400 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

cs42888_supply: 3300 mV

vio1: 3300 mV

vio2: 3300 mV

vd: 3300 mV

va: 5000 mV

platform usb_h1_vbus.33: Driver reg-fixed-voltage requests probe deferral

platform usb_otg_vbus.34: Driver reg-fixed-voltage requests probe deferral

3P3V: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

pureg-dummy: no parameters

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 5, 131072 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP: reno registered

UDP hash table entries: 1024 (order: 3, 32768 bytes)

UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 708K (85000000 - 850b1000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

mxc_epit: probe of 20d0000.epit failed with error -22

mxc_epit: probe of 20d4000.epit failed with error -22

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

console [pstore-1] enabled

ramoops: attached 0x100000@0x8bf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink socket (disabled)

type=2000 audit(0.490:1): initialized

bounce pool size: 64 pages

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 3498

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

MIPI DSI driver module loaded

mxc_hdmi 20e0000.hdmi_video: hdcp disable

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init

mxc_hdmi_disp_init: JAi Khirod

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init - default mode 640x480M@60 bpp=32

mxc_hdmi 20e0000.hdmi_video: Enabled HDMI clocks

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 640x480@60: CVT Name - .307M3

Ranjini printing &m in disp_init

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini printing cmode table...

fb_videomode = 120 1280 720 6734 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff -1

Ranjini d ... 880

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 100 1280 720 6734 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 30 1920 1080 13468 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 25 1920 1080 13468 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 24 1920 1080 13468 148 638 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1920 1080 6734 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1280 720 13468 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 176

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 176Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 1920 1080 6734 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1280 720 13468 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 880Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 80

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 80

Ranjini d ... 80Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 80

Ranjini d ... 0

Ranjini Best found if condition........... = 0

Ranjini Finally Returning best .......... = 0

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init exit

mxc_hdmi 20e0000.hdmi_video: Ranjini mxc_hdmi_disp_init exit ret before err 0

mxc_dispdrv_gethandle,driver initialization entry=0

hdmi Ranjini..........mxc_dispdrv_gethandle List  name hdmi Ranjini..........mxc_dispdrv_gethandle name

mxcfb_dispdrv_init, khiroddisplay driver handle: ret=-734542400mxc_sdc_fb fb.23: registered mxc display driver hdmi

fb_match_mode, khirodmode equal value: m=-734537080

fb_match_mode, khirodmode equal value: m=-734537144

fb_match_mode, khirodmode equal value: m=-734537208

fb_match_mode, khirodmode equal value: m=-734537272

fb_match_mode, khirodmode equal value: m=-734537336

fb_match_mode, khirodmode equal value: m=-734537400

fb_match_mode, khirodmode equal value: m=-734537464

fb_match_mode, khirodmode equal value: m=-734537528

fb_match_mode, khirodmode equal value: m=-734537592

fb_match_mode, khirodmode equal value: m=-734537656

fb_match_mode, khirodmode equal value: m=-734537720

fb_match_mode, khirodmode equal value: m=-734537784

fb_match_mode, khirodmode equal value: m=-734537848

fb_match_mode, khirodmode equal value: m=-734537912

fb_match_mode, khirodmode equal value: m=-734537976

fb_match_mode, khirodmode equal value: m=-734538040

fb_match_mode, khirodmode equal value: m=-734538104

fb_match_mode, khirodmode equal value: m=-734538168

fb_match_mode, khirodmode equal value: m=-734538232

fb_match_mode, khirodmode equal value: m=-734538296

fb_match_mode, khirodmode equal value: m=-734538360

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init

mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE

Ranjini FB_EVENT_MODE_CHANGE .. mode

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini FB_EVENT_MODE_CHANGE .. &hdmi->previous_non_vga_mode

fb_videomode = 0 0 0 0 0 0 0 0 0 0 0 0 0

Ranjini hdmi->fb_reg 0

mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_BLANK - UNBLANK

fb_match_mode, khirodmode equal value: m=-734537080

fb_match_mode, khirodmode equal value: m=-734537144

fb_match_mode, khirodmode equal value: m=-734537208

fb_match_mode, khirodmode equal value: m=-734537272

fb_match_mode, khirodmode equal value: m=-734537336

fb_match_mode, khirodmode equal value: m=-734537400

fb_match_mode, khirodmode equal value: m=-734537464

fb_match_mode, khirodmode equal value: m=-734537528

fb_match_mode, khirodmode equal value: m=-734537592

fb_match_mode, khirodmode equal value: m=-734537656

fb_match_mode, khirodmode equal value: m=-734537720

fb_match_mode, khirodmode equal value: m=-734537784

fb_match_mode, khirodmode equal value: m=-734537848

fb_match_mode, khirodmode equal value: m=-734537912

fb_match_mode, khirodmode equal value: m=-734537976

fb_match_mode, khirodmode equal value: m=-734538040

fb_match_mode, khirodmode equal value: m=-734538104

fb_match_mode, khirodmode equal value: m=-734538168

fb_match_mode, khirodmode equal value: m=-734538232

fb_match_mode, khirodmode equal value: m=-734538296

fb_match_mode, khirodmode equal value: m=-734538360

Console: switching to colour frame buffer device 80x30

mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_FB_REGISTERED

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_fb_registered

mxc_sdc_fb fb.24: Can't get fb option for mxcfb1!

mxc_sdc_fb fb.25: Can't get fb option for mxcfb2!

mxc_dispdrv_gethandle,driver initialization entry=0

ldb Ranjini..........mxc_dispdrv_gethandle List  name ldb Ranjini..........mxc_dispdrv_gethandle name

mxcfb_dispdrv_init, khiroddisplay driver handle: ret=-734545984mxc_sdc_fb fb.26: registered mxc display driver ldb

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected

Ranjini Entering mxc_hdmi_read_edid....

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid

unable to read EDID block

mxc_hdmi 20e0000.hdmi_video: read failed

Ranjini Entering mxc_hdmi_read_edid Failing HDMI_EDID_FAIL....

Ranjini .... mxc_hdmi_read_edid edid status ...is -1mxc_hdmi 20e0000.hdmi_video: Read EDID again

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: initialized

imx-sdma 20ec000.sdma: loaded firmware 1.1

pfuze100-regulator 0-0008: Full lay: 1, Metal lay: 1

pfuze100-regulator 0-0008: FAB: 0, FIN: 0

pfuze100-regulator 0-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV

pfuze100-regulator 0-0008: ramp failed, err -5

SW1C: failed to set ramp_delay

pfuze100-regulator 0-0008: register regulatorSW1C failed

pfuze100-regulator: probe of 0-0008 failed with error -5

Serial: IMX driver

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

Ranjini Entering mxc_hdmi_read_edid....

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid

unable to read EDID block

mxc_hdmi 20e0000.hdmi_video: read failed

Ranjini Entering mxc_hdmi_read_edid Failing HDMI_EDID_FAIL....

Ranjini ... Coming to default..

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_default_modelist

mxc_hdmi 20e0000.hdmi_video: create default modelist

Ranjini printing cmode table...

fb_videomode = 120 1280 720 6734 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff -1

Ranjini d ... 880

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 100 1280 720 6734 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 880

Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 30 1920 1080 13468 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 1880

Ranjini printing cmode table...

fb_videomode = 25 1920 1080 13468 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 1880

Ranjini printing cmode table...

fb_videomode = 24 1920 1080 13468 148 638 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 1880

Ranjini printing cmode table...

fb_videomode = 50 1920 1080 6734 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 1880

Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 896

Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 896

Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 992

Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 992

Ranjini printing cmode table...

fb_videomode = 50 1280 720 13468 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 880

Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 880

Ranjini d ... 176

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 176

Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 1920 1080 6734 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 1880

Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 800

Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 800

Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 1040

Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 1040

Ranjini printing cmode table...

fb_videomode = 60 1280 720 13468 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 880

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 176

Ranjini d ... 80

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 80

Ranjini d ... 80

Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini diff 80

Ranjini d ... 0

Ranjini Best found if condition........... = 0

Ranjini Finally Returning best .......... = 0

fb_match_mode, khirodmode equal value: m=-733705272

fb_match_mode, khirodmode equal value: m=-733705336

fb_match_mode, khirodmode equal value: m=-733705400

fb_match_mode, khirodmode equal value: m=-733705464

fb_match_mode, khirodmode equal value: m=-733705528

fb_match_mode, khirodmode equal value: m=-733705592

fb_match_mode, khirodmode equal value: m=-733705656

fb_match_mode, khirodmode equal value: m=-733705720

fb_match_mode, khirodmode equal value: m=-733705784

fb_match_mode, khirodmode equal value: m=-733705848

fb_match_mode, khirodmode equal value: m=-733705912

fb_match_mode, khirodmode equal value: m=-733705976

fb_match_mode, khirodmode equal value: m=-733706040

fb_match_mode, khirodmode equal value: m=-733706104

fb_match_mode, khirodmode equal value: m=-733706168

fb_match_mode, khirodmode equal value: m=-733706232

fb_match_mode, khirodmode equal value: m=-733706296

fb_match_mode, khirodmode equal value: m=-733706360

fb_match_mode, khirodmode equal value: m=-733706424

fb_match_mode, khirodmode equal value: m=-733706488

console [ttymxc3] enabled

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

si476x-core 0-0063: Using default platform data.

si476x-core 0-0063: No IRQ number specified, will use polling

si476x-core 0-0063: Error while sending command 0x11

si476x-core 0-0063: The device in inconsistent power state

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <[email protected]>

CAN device driver interface

flexcan 2094000.can: device registered (reg_base=f01e8000, irq=143)

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

fb_match_mode, khirodmode equal value: m=-733706552

fb_match_mode, khirodmode equal value: m=-733705272

fb_match_mode, khirodmode equal value: m=-733705336

fb_match_mode, khirodmode equal value: m=-733705400

fb_match_mode, khirodmode equal value: m=-733705464

fb_match_mode, khirodmode equal value: m=-733705528

fb_match_mode, khirodmode equal value: m=-733705592

fb_match_mode, khirodmode equal value: m=-733705656

fb_match_mode, khirodmode equal value: m=-733705720

fb_match_mode, khirodmode equal value: m=-733705784

fb_match_mode, khirodmode equal value: m=-733705848

fb_match_mode, khirodmode equal value: m=-733705912

fb_match_mode, khirodmode equal value: m=-733705976

fb_match_mode, khirodmode equal value: m=-733706040

fb_match_mode, khirodmode equal value: m=-733706104

fb_match_mode, khirodmode equal value: m=-733706168

fb_match_mode, khirodmode equal value: m=-733706232

fb_match_mode, khirodmode equal value: m=-733706296

fb_match_mode, khirodmode equal value: m=-733706360

fb_match_mode, khirodmode equal value: m=-733706424

fb_match_mode, khirodmode equal value: m=-733706488

fb_match_mode, khirodmode equal value: m=-733706552

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

fb_match_mode, khirodmode equal value: m=-733705272

fb_match_mode, khirodmode equal value: m=-733705336

fb_match_mode, khirodmode equal value: m=-733705400

fb_match_mode, khirodmode equal value: m=-733705464

fb_match_mode, khirodmode equal value: m=-733705528

fb_match_mode, khirodmode equal value: m=-733705592

fb_match_mode, khirodmode equal value: m=-733705656

fb_match_mode, khirodmode equal value: m=-733705720

fb_match_mode, khirodmode equal value: m=-733705784

fb_match_mode, khirodmode equal value: m=-733705848

fb_match_mode, khirodmode equal value: m=-733705912

fb_match_mode, khirodmode equal value: m=-733705976

fb_match_mode, khirodmode equal value: m=-733706040

fb_match_mode, khirodmode equal value: m=-733706104

fb_match_mode, khirodmode equal value: m=-733706168

fb_match_mode, khirodmode equal value: m=-733706232

fb_match_mode, khirodmode equal value: m=-733706296

fb_match_mode, khirodmode equal value: m=-733706360

fb_match_mode, khirodmode equal value: m=-733706424

fb_match_mode, khirodmode equal value: m=-733706488

fb_match_mode, khirodmode equal value: m=-733706552

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

platform 2184000.usb: Driver imx_usb requests probe deferral

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

platform 2184200.usb: Driver imx_usb requests probe deferral

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

usbcore: registered new interface driver wacom

egalax_ts 0-0004: Failed to wake up, disable suspend,otherwise it can not wake up

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

egalax_ts 0-0004: Failed to read firmware version

egalax_ts: probe of 0-0004 failed with error -5

input: isl29023 light sensor as /devices/virtual/input/input0

isl29023 1-0044: driver version 1.0 enabled

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

DBG sensor data is at 80fc48a0

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode

Ranjini printing cmode table...

fb_videomode = 120 1280 720 6734 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff -1

Ranjini d ... 880

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 100 1280 720 6734 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 30 1920 1080 13468 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 25 1920 1080 13468 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 24 1920 1080 13468 148 638 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1920 1080 6734 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1280 720 13468 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 880

Ranjini d ... 176

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 176Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 1920 1080 6734 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1280 720 13468 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 880Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 176

Ranjini d ... 80

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 80

Ranjini d ... 80Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 42105 80 16 3 13 64 4 2 0 32

Ranjini diff 80

Ranjini d ... 0

Ranjini Best found if condition........... = 0

Ranjini Finally Returning best .......... = 0

Ranjini fb_find_nearest_mode

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini Printing non_vga_mode

fb_videomode = 0 0 0 0 0 0 0 0 0 0 0 0 0

Ranjini Printing mode

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed

Ranjini printing cmode table...

fb_videomode = 120 1280 720 6734 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff -1

Ranjini d ... 880

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 100 1280 720 6734 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 30 1920 1080 13468 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 25 1920 1080 13468 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 24 1920 1080 13468 148 638 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1920 1080 6734 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1280 720 13468 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 176

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 176Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 1920 1080 6734 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1280 720 13468 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 880Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 80

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 80

Ranjini d ... 80Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 80

Ranjini d ... 0

Ranjini Best found if condition........... = 0

Ranjini Finally Returning best .......... = 0

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=1

mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer

mxc_hdmi 20e0000.hdmi_video: final pixclk = 24780000

mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode

mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk

mxc_hdmi 20e0000.hdmi_video: set up AVI frame

Ranjini printing cmode table...

fb_videomode = 120 1280 720 6734 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff -1

Ranjini d ... 880

Ranjini Best found if condition........... = 0

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video17

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video18

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video19

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

gspca_main: v2.14.0 registered

mag3110 1-000e: check mag3110 chip ID

Ranjini printing cmode table...

fb_videomode = 100 1280 720 6734 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

input: FreescaleMagnetometer as /devices/virtual/input/input1

input: eCompass as /devices/virtual/input/input2

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 30 1920 1080 13468 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...mag3110 1-000e: mag3110 is probed

fb_videomode = 25 1920 1080 13468 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 24 1920 1080 13468 148 638 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1920 1080 6734 148 528 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 576 18518 136 24 39 5 128 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 896Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...

fb_videomode = 50 1440 288 37037 138 24 19 2 126 3 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 992Ranjini printing cmode table...input: FreescaleAccelerometer as /devices/virtual/input/input3

mma8x5x device driver probe successfully

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: [email protected]

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

fb_videomode = 50 1280 720 13468 220 440 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 880Ranjini Best found else condition........... = 0

Ranjini printing cmode table...mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

Galcore version 5.0.11.25762

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 880

Ranjini d ... 176

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 50 720 576 37037 68 12 39 5 64 5 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 176Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 1920 1080 6734 148 88 36 4 44 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1880Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 480 18500 120 32 30 9 124 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 800Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1440 240 37108 114 38 15 4 124 3 0 16 0

mmc2: Problem setting current limit!

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 1040Ranjini printing cmode table...

fb_videomode = 60 1280 720 13468 220 110 20 5 40 5 3 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 880Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 32 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 176

Ranjini d ... 80

Ranjini Best found if condition........... = 0

Ranjini printing cmode table...

fb_videomode = 60 720 480 37037 60 16 30 9 62 6 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 80

Ranjini d ... 80Ranjini Best found else condition........... = 0

Ranjini printing cmode table...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 0

Ranjini printing mode we are searching...

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini diff 80

Ranjini d ... 0

Ranjini Best found if condition........... = 0

Ranjini Finally Returning best .......... = 0

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit

mmc2: new ultra high speed DDR50 SDHC card at address aaaa

mmcblk2: mmc2:aaaa SL16G 14.8 GiB

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected exit

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk2: p4 size 28936192 extends beyond EOD, truncated

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

cs42xx8 0-0048: found device, revision 4

snd-soc-dummy snd-soc-dummy: ASoC: Failed to create platform debugfs directory

imx-cs42888 sound-cs42888.36:  cs42888 <-> 2024000.esai mapping ok

imx-cs42888 sound-cs42888.36:  snd-soc-dummy-dai <-> asrc_p2p.3 mapping ok

imx-cs42888 sound-cs42888.36:  cs42888 <-> 2024000.esai mapping ok

imx-spdif sound-spdif.39:  dir-hifi <-> 2004000.spdif mapping ok

imx-audio-hdmi sound-hdmi.38:  hdmi-hifi <-> hdmi_audio.17 mapping ok

imx-tuner-si476x sound-fm.37: failed to find FM platform device

imx-tuner-si476x: probe of sound-fm.37 failed with error -22

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (16384 buckets, 65536 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

regulator-dummy: disabling

imx mcc test is registered.

usb_h1_vbus: 5000 mV

usb_otg_vbus: 5000 mV

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.53 ehci_hcd

usb usb1: SerialNumber: ci_hdrc.1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.20 as /devices/soc0/gpio-keys.20/input/input4

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:49:08 UTC (2948)

ALSA device list:

  #0: cs42888-audio

  #1: imx-spdif

  #2: imx-hdmi-soc

Freeing unused kernel memory: 336K (80e7c000 - 80ed0000)

type=1403 audit(2948.760:2): policy loaded auid=4294967295 ses=4294967295

type=1404 audit(2948.770:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: /init.rc: 456: invalid command 'mknod'

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

EXT4-fs (mmcblk2p5): barriers disabled

EXT4-fs (mmcblk2p5): recovery complete

EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: barrier=0

fs_mgr: __mount(source=/dev/block/mmcblk2p5,target=/system,type=ext4)=0

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p4): recovery complete

EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p6): recovery complete

EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0

binder: 144:144 transaction failed 29189, size 0-0

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

android_usb: already disabled

read descriptors

read strings

mtp_bind_config

root@sabreauto_6q:/ # android_work: sent uevent USB_STATE=CONNECTED

ci_hdrc ci_hdrc.0: freeing queued request

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

android_usb gadget: high-speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

healthd: No battery devices found

fb_match_mode, khirodmode equal value: m=-733705272

fb_match_mode, khirodmode equal value: m=-733705336

fb_match_mode, khirodmode equal value: m=-733705400

fb_match_mode, khirodmode equal value: m=-733705464

fb_match_mode, khirodmode equal value: m=-733705528

fb_match_mode, khirodmode equal value: m=-733705592

fb_match_mode, khirodmode equal value: m=-733705656

fb_match_mode, khirodmode equal value: m=-733705720

fb_match_mode, khirodmode equal value: m=-733705784

fb_match_mode, khirodmode equal value: m=-733705848

fb_match_mode, khirodmode equal value: m=-733705912

fb_match_mode, khirodmode equal value: m=-733705976

fb_match_mode, khirodmode equal value: m=-733706040

fb_match_mode, khirodmode equal value: m=-733706104

fb_match_mode, khirodmode equal value: m=-733706168

fb_match_mode, khirodmode equal value: m=-733706232

fb_match_mode, khirodmode equal value: m=-733706296

fb_match_mode, khirodmode equal value: m=-733706360

fb_match_mode, khirodmode equal value: m=-733706424

fb_match_mode, khirodmode equal value: m=-733706488

fb_match_mode, khirodmode equal value: m=-733706552

mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure

mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE

Ranjini FB_EVENT_MODE_CHANGE .. mode

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini FB_EVENT_MODE_CHANGE .. &hdmi->previous_non_vga_mode

fb_videomode = 59 640 480 39722 48 16 33 10 96 2 0 16 32

Ranjini hdmi->fb_reg 1

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

warning: `main' uses 32-bit capabilities (legacy support in use)

period 102593883 ,timeout is 102602473, wake up is :0

period 102593883 ,timeout is 102602473, wake up is :0

request_suspend_state: wakeup (3->0) at 19292101001 (1970-01-01 00:49:21.573591334 UTC)

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

acc_open

acc_release

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

mtp_open

binder: undelivered transaction 3728

ERROR: unrecognized std! ffffff (PAL=ff, NTSC=b000

period 66 ,timeout is 0, wake up is :0

mma enable setting active

mma enable setting inactive

request_suspend_state: sleep (0->3) at 48159590671 (1970-01-01 00:49:50.441081004 UTC)

active wake lock gadget

Regards,

Prasad

0 件の賞賛
返信
4 返答(返信)

1,931件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Prasad,

This cable converters from HDMI to VGA does not work if both of your devices that you are trying to attach had both interfaces, since the VGA it is an Analog signal and the HDMI it is a Digital one.  A cable it is not enough to make the change you need a black box to make this happens

0 件の賞賛
返信

1,931件の閲覧回数
prasads
Contributor I

Hi, i also try by

connecting hdmi cabke to tv from board.i was geting in log like edid data

read failed.

Regards, Prasad

0 件の賞賛
返信

1,931件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

which one has the HDMI the TV or the i.MX?.  The TV most have both  Inputs HDMI and VGA and this way it works.

0 件の賞賛
返信

1,931件の閲覧回数
prasads
Contributor I

Hi james,

i connect the HDMI cable to tv in HDMI mode.previously I also getting

display by connecting this converter cable from wandboard to VGA

monitor.but in Sabre auto quad board,i did not get any display.

Regards

Prasad

On Mon, Feb 8, 2016 at 11:36 PM, jamesbone <[email protected]>

0 件の賞賛
返信